I use a 2s configuration which is configured through the "CELL_BATPREZ" pin. This pin has according to the datasheet also the function to detect a removed battery by forcing the voltage to a maximum of 15% of the VDDA(or REGN). I can not get the pin to respond accordingly? I use the EVM to ensure that my design will work in the future and this could save a troublesome mechanical switch.
Jørgen Olsen