This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ27742-G1: Learning cycle complete. I think

Part Number: BQ27742-G1

So the start button is still grayed out with cancel my only option.  However my results show:

Wed Oct 25 13:06:08 EDT 2017: Learning cycle started...
Wed Oct 25 13:06:08 EDT 2017: Start task: Discharge ( TerminateVoltage = 3300 mV )
Wed Oct 25 13:49:39 EDT 2017: End task: Discharge completed in 00:43:30
Wed Oct 25 13:49:39 EDT 2017: Start task: Relax ( Duration = up to 360 minutes )
Wed Oct 25 15:46:13 EDT 2017: End task: Relax completed in 01:56:34
Wed Oct 25 15:46:13 EDT 2017: Start task: Charge ( FC/TC Bit = true )
Wed Oct 25 19:08:40 EDT 2017: End task: Charge completed in 03:22:27
Wed Oct 25 19:08:40 EDT 2017: Start task: Relax ( Duration = up to 120 minutes )
Wed Oct 25 19:41:25 EDT 2017: End task: Relax completed in 00:32:44
Wed Oct 25 19:41:25 EDT 2017: Start task: Discharge ( TerminateVoltage = 3300 mV )
Thu Oct 26 19:10:02 EDT 2017: End task: Discharge completed in 23:28:36
Thu Oct 26 19:10:02 EDT 2017: Start task: Relax ( Duration = up to 360 minutes )
Thu Oct 26 22:24:13 EDT 2017: End task: Relax completed in 03:14:11
Thu Oct 26 22:24:14 EDT 2017: Learning cycle completed!
Thu Oct 26 22:24:14 EDT 2017: Learning cycle was successful!

And my pack capacity looks reasonable.  If this worked how do I export everything so I can program other packs?  Is it enough to just do the export golden image function?

Thank you