Other Parts Discussed in Thread: UCD9090
I'm trying to make sure I'm clear on this device's capabilities and I'm finding inconsistencies in the datasheet and web-descriptions.
The UCD9090-Q1 is titled as a "10-Rail Power-Supply Sequencer and Monitor With ACPI Support". But it seems to have 11 monitor inputs which would indicate the ability to monitor more than 10 voltages. Page 15 of the datasheet expands on the 11 monitor inputs and then in the following paragraph talks about the 12 voltages that the chip can monitor. Playing with the Fusion Designer software It seems like you can only configure the part to monitor 10 power rails which points back to only 10 monitors but there is still that's 11th monitor input....... o_O
So, which is it: 10, 11, or 12? If it's 10 what's the Mon11 input for?
Thanks.