This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5116: Undershoot @ LO-GND or HO-SW

Part Number: LM5116

Dear Team,

our customer sees a negative undershoot with about -1.5V @ LO-GND or HO-SW for ~5ns.

The specs of the device mention a max value of -0.3V.

Is this short undershoot a problem for the device?

Are there recommendations how to lower such an undershoot, like a snubber or cap?

Thanks and best Regards
Martin

  • I do not support LM5116 directly, but I can tell you it is practically impossible to eliminate these types of switching transients.  The -0.3 V specification is most likely a dc specification taken directly from the process specification.  Many of our devices have a transient specification in the absolute maximum table to cover this situation.  For some reason, LM5116 does not address this.

  • Hello John,
    great, thanks for the answer.
    I will look tomorrow for a similar part, just to get a feeling of the ball park what the spec allows.

    Question to a colleague who supports the device: Should we take care of the transient or is it still in an acceptable range?

    Thanks and best regards
    Martin
  • Hi Martin,

    The transient specs you provided do not pose an issue for the LM5116.

    Regards,

    Tim