This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27714: Driver IC with 800V+ , 4A double channel

Part Number: UCC27714
Other Parts Discussed in Thread: UCC21520-Q1

Hello

I need a driver IC for DC/DC converter with input handling up to 800V/900V or more; 4A current is required for high and low side with automative grade. I have got UCC27714 matching to my requirement with highest voltage available. Can you suggest me other part number available according to my requirement.?

Thanks in advance.

Regards

Tanvi Mahajan