Other Parts Discussed in Thread: BQ2002
Hello,
In the BQ2002E datasheet, it states that Starting A Charge Cycle can be initiated two ways, I am interested in the 2nd method, bringing the BAT pin below Vmcv (2.0V).
I am implementing a 2 NiMH cell with a 5V source supply. I am having trouble restarting a Charge Cycle by using a small FET to pull the BAT pin to ground through the resistive divider (R14 in the SLUU007B example). I have a resistive divider on the BAT pin of 475k and 475k.
I am confused by the example schematic in SLUU007B. If you assume that you are using the "4 CELLS" divider, R9 + R14 (301k + 100k), in order to reach Vmcv(2.0V), BAT+ would need to be 8.0V. How would a 4 Cell NiMH battery ever reach that voltage?
What am I missing here?
...kevin