Other Parts Discussed in Thread: , TPS3890, TPS3890-Q1
Team,
My customer has the following inquiry:
"I’d like to use the TPS3808G01 in a new design to monitor a 1.5V supply rail. I cannot use the TPS3808G15 because my minimum supply voltage is 1.425V. (It’s supplying a Microsemi A3P1000) The datasheet for the TPS3808, section 7.5 states a Vit tolerance of bormal operation, setween 2% and -2%. My supply voltage may drop to 1.474V in no I can’t accommodate that window of 4%. Could I ask you just how might parts be distributed in that 2% to -2% range? If it’s a Normal/Gaussian distribution, then might I expect a better accuracy in reality?"
Is there a better part we should be using?
Regards,
Aaron