In regards to Max Error % for BQ impedance tracking fuel gauges.
How is Percentage RSOC calculated with max error %?
Is it multiplied or added?
i.e:. %RSOC * max error%
Assuming it is multiplied:
If RSoC% is 50% and max error% is 10%:
RSoC error calculated: 0.5 * 0.1 = 0.05 (100%) => 5%
How is that 5% calculated with RsoC%?
Is it 5% +/-? Such as: 47.5% to 52.5%? or 45% to 55%?
Application notes, technical reference, and data sheets do not clearly specify this.
Also, does max error % affect or point to any other parameter other than RSOC... such as calibration?
Thanks,
Kelsey