This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76PL455A: Delay of about 300uS when BQ transmits data

Part Number: BQ76PL455A


Dear All, 

So what i am seeing is that there is an ~delay of 300uS when i read the cell data from BQ device which i don't see when using BQ EVM with BQ GUI. Can someone help me figure out why this delay is there ? 

Read Cell data is divided ito differents case states to read the data and it does it as follows.

Step 1 - broadcast sample and store command 

Step 2 - Read cell data 1 to 8

Step 3 - Read cell data 9 to 16

Step 4 - Read Aux data 1 to 8

Step 5 - Go back to step 2 and read data for next device in the stack. 

I have cross check it several times but i can't figure out where is the delay coming from. I have also set the TX_HOLDOFF time to 0.

Your help will be very much appreciated, so can you please help ? 

Kind Regards

Vikram Jain