Other Parts Discussed in Thread: LM26484, LP873222-Q1, LP873220-Q1
Hello,
The LM26480 looks to be an almost perfect fit for an application of mine, but the 1.5A on rail 1 is a little tight. Otherwise the 1.5A on rail 2 and the two LDOs at 300 mA are ideal ( along with their voltage ranges ).
Is there something in the catalog that acts like LM26480 but has more current on rail 1? Please point out your closest match. Also, I like the low cost and discrete enable signals, but I can do I2C if need be.
Also, is there a way to cheat and have 1.8A on rail 1 and 1.2A on rail 2 ( still 3.0A total for both bucks )?
Thank you,
Bob