This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z100: BQ27541 Control Command communication using HDQ interface

Part Number: BQ34Z100

We wanted to know about how control command and its subsequent byte sub commands to retrieve data using the HDQ interface . We use HDQ over UART 

We are successfully able to Read other standard commands like Voltage(0x08/0x09) AverageCurrent(0x0A/0x0B) and we follow the below protocol for that

1 .Read high byte (H0)

2. Read low byte (L0)

3. Read high byte again (H1)

4. If H1 = H0, then the valid 16-bit result is H0:L0 5. Otherwise, read low byte again (L1) and the valid 16-bit result is H1:L1.

This procedure is sufficient to guarantee that the 16-bit word is read correctly

Please help us with the right protocol for sending CONTROL command and the subsequent sub command like "CHEM ID: 0x0008 ,FW_VERSION: 0x0002  " for retrieving these data .

We use HDQ protocol 


Does sealed or unsealed have anything to do with these basic sub commands  ?