Hi
I have project for designing wire and wireless intergrated charge with bellow requirement:
1. Left Qi charger is for blue tooth headset. Coil has to be no more than 32mm (W) x 32 mm (H).
2. Right Qi charger needs to inductive charge mobile phone. Coil has to be no more than 36mm (W) x 36 mm (H).
To the right of Qi chargers is
3. 1 x USB 3.0 port 5v 2A
4. 1 x USB C port5v 2A
Also ,need to be able to power all 4 at same time.
And finally ,component is a power port to get current from the mains...
Can I get a reference design for each sections , to intergrated all in one charge?
Thanks
p/s: I tried to looking in wireless charge forum, but i can not post in here.