This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28700: SLUC408B spreadsheet

Part Number: UCC28700


Hello,

I'm using the SLUC408B spreadsheet to calculate the BoM parameters for an isolated flyback DCDC based on UCC28700.

In this XL sheet, on line 121 we Estimate the FET switching losses with the following formulae:

=(Vfly-(Vout+Vdg)*NpNs)*Ippk*C116*fmax/2

Shouldn't it be

=(Vfly+(Vout+Vdg)*NpNs)*Ippk*C116*fmax/2  ?

And another point: I don't have any Fusable Resistor in my design, so I would like to put zero in line 80 but the spreasheet cell is locked. Is it possible to unlock it ?

Also the Input Ripple is locked (line 62). I would like to change it as I use a DC input for this design.

... and the maximum drain voltage of the FET (line 113) as I use a higher voltage FET

Thank you

  • Boris,

    Thanks for your interest in TI here. I've contacted an applications engineer to answer your questions. You should hear back soon.

    Regards

    John

  • Boris,

    Most of these are locked and simplified for most customers to make some common assumptions to make it easier for you as a user. You sound like a more experienced user who prefers to be in control of each detail on the design. :)

    I believe Bernard Keogh contacted you through email on this on how to unlock and edit the calculator. Do you have further questions on this or have we resolved your questions?