Other Parts Discussed in Thread: TPS2378, LM5116, UCC2897A, TPS23754, TPS23751
Hey IEEE community!
my question is the following: What is the main difference between PD controller only and PD controller and DC/DC converter?
Thank you!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Amina,
A "PD-only" controller is less integrated than a "PD controller plus DC/DC converter."
The PD-only controller (example: TPS2378) provides the system with a way to complete core PoE functions (detection and classification of a load) through communication with the PSE. However, it requires coupling with a DC/DC PWM solution - such as the LM5116 or UCC2897A - for the power stage.
PD controllers which integrate the DC/DC converter (examples: TPS23751, TPS23754) can enable smaller form factor PCBs (1 less part) and, in some cases, a lower overall system cost than the 2-chip approach.
With that said, selecting a PD-only controller enables greater flexibility across a platform of models - say, one model where cost is the #1 objective (and can partner with a flyback PWM) and one that cares more about efficiency (and can partner with an active bridge PWM). In this business model, one PD-only controller can be qualified (such as the TPS2378) and used across multiple platforms.
TI offers both options in order to deliver a flexible suite of PoE options.
Thank you for your interest in TI PoE solutions!