This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD90240: Setting GPIO pins to open drain?

Part Number: UCD90240


When using this chip in Fusion Digital Power Designer I am having trouble setting the GPIO pins (GPIO1-24) to the open drain configuration. Most of the devices that I am connected to are 1.8V IO so open drain in conjunction with pull ups works best for my application. The note on the side of the program infers that I can do this but I don't see how.