This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61099: Inductance at light load

Part Number: TPS61099

Hi, team.

TPS61099 is used in 1.2Vin 2.0Vout.

A load current is light at less than 15mA, so it works in DCM only.

The inductance of the recommendation is 1.0uH in case of less than 3 Vout, but is 1.0uH also always preferred in DCM?

What is the risk when using 2.2uH?

BR