This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25145: LM25145 no loading

Part Number: LM25145


Dear  All:

     I use  the LM25145RGY to design DC-DC circuit   

    Condition:   input voltage :24V

                         output voltage :12.6v

                        no  loading

      I  find  the  input  current  can reach 15ma, but  my product requirements can only go to the 5ma. can the   LM25145RGY  meet the requirement. Thanks!