This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25504: 5V operation w/ <10kOhm load on VSTOR

Part Number: BQ25504

I am struggling to get the BQ25504 to provide a regulated 5.1V on VSTOR when I have <10kOhm resistor to GND on this pin.  On the input to the BQ25504 I have a 3.0V Zener diode, 10uF cap to GND and a nonlinear load resistor that varies between 80kOhms (0.1V)-500kOhms (3V).

I am using the following values from the schematic on the datasheet (Figure 14 - Typical Solar Application Circuit).

U2 BQ25504
L1 22uH, 0805, 100mA
D1 3.0V Zener Diode
CBYP 0.01uF, 0603, 10V
CSTOR 4.7uF, 0805, 10V
CREF 0.01uF, 0603, 10V
ROC1 10M
ROC2 10M
ROV1 3.6MHOHM, 0402
ROV2 6.49MOHM, 0402
RUV1 3.0MOHM, 0402
RUV2 6.98MOHM, 0402
ROK1 2.8MOHM, 0402
ROK2 6.98MOHM, 0402
ROK3 220K, 0402

I have an 820uF electrolytic cap on VBAT.

When I have an open circuit on VSTOR the circuit starts up nicely. When I have a 10kOhm resistor on VSTOR to GND then I can't get the circuit to start up.  Any recommendations would be welcome.