Hello everyone,
I use the UCC27211 in my project. In particular, I make the electrical circuit as in the datasheet in the half bridge configuration. In this moment, the Vhi and Vli pins are connected to ground and the Vhs pin is not connected to the transformer. I use 9V for UCC27211 and variable boot voltage from 6V to 24V for half bridge mosfet.
My problem is on Vhs pin because I always measure a constant voltage (close to the supply voltage). But if Vhi and Vli are at logical level voltage, in Vhs the voltage it should be zero. It's right?
If I disconnect the high side mosfet, the voltage on Vhs is always present.
Please, can anyone help me?
Thank you
Best Regards,
Donatello