This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I would like to input 5 V and get an output of 7.3 V. I need a max output current of 2 A. For part PTN04050CAH and PTN04050CAD the maximum output current at this voltage is too low. Am I able to connect two of these devices in parallel in order to achieve my desired current output?