This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS562201: About inductor selection

Part Number: TPS562201
Other Parts Discussed in Thread: TPS561201

Hi,

I made a board using the TPS562201 device.
The specification is below.
I am using the constant of the inductor described in the datasheet. It is 4.7uH.
However, since the inductor ripple current is large, we want to change the value of the inductor to reduce the influence of noise.
The MAX value of the inductor at the output voltage of 5V is indicated in the data sheet and its value is 4.7uH.
I would like to use the 6.8uH inductor with the following model number.
The output capacitor is 30uF.

Is it possible to use a 6.8μF inductor?

Best Regards,


(specification)
VIN : 12V
VOUT : 5 V
IOUT : 1A

(Inductor to change)
SWPA4030S6R8MT:6.8μH, SHENZHEN SUNLORD