This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34110: BQ34110

Part Number: BQ34110

Hello,

I am trying to use BQ34110 on 10 cells NiMH batteries, to do that I followed the Guide for CEDV Data collection (SLUUB45A).

I sent you Data Log and Config files and I received from you different files: GPC_CEDV and OCV11.

On GPC_CEDV file, there are 10 parameters:

EMF 1322
EDVC0 425
EDVC1 0
EDVR1 1
EDVR0 76
EDVT0 3373
EDVTC 9
VOC75 13000
VOC50 12730
VOC25 12380

On .gg files, I put the paramters as:

"Gas Gauging","CEDV Profile","EMF","1322","-"
"Gas Gauging","CEDV Profile","C0","425","-"
"Gas Gauging","CEDV Profile","R0","76","-"
"Gas Gauging","CEDV Profile","T0","3373","-"
"Gas Gauging","CEDV Profile","R1","1","-"
"Gas Gauging","CEDV Profile","TC","9","-"
"Gas Gauging","CEDV Profile","C1","0","-"

On which lines of .gg files, I must put the 3 parameters:

VOC75 13000 
VOC50 12730 
VOC25 12380

On OCV11 file, there are 11 parameters

SOC, % OCV, mV
0        1001
10      1221
20      1250
30      1266
40      1274
50      1281
60      1286
70      1291
80      1301
90      1329
100    1400

On which lines of .gg files, I must put the 11 parameters, is it on:

"Gas Gauging","CEDV Profile","Voltage 0% DOD","1400","mV"
"Gas Gauging","CEDV Profile","Voltage 10% DOD","1329","mV"
"Gas Gauging","CEDV Profile","Voltage 20% DOD","1301","mV"
"Gas Gauging","CEDV Profile","Voltage 30% DOD","1291","mV"
"Gas Gauging","CEDV Profile","Voltage 40% DOD","1286","mV"
"Gas Gauging","CEDV Profile","Voltage 50% DOD","1281","mV"
"Gas Gauging","CEDV Profile","Voltage 60% DOD","1274","mV"
"Gas Gauging","CEDV Profile","Voltage 70% DOD","1266","mV"
"Gas Gauging","CEDV Profile","Voltage 80% DOD","1250","mV"
"Gas Gauging","CEDV Profile","Voltage 90% DOD","1221","mV"
"Gas Gauging","CEDV Profile","Voltage 100% DOD","1001","mV"

Thank for your help

Best regards

Serge