This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS549D22: Power sequence, PMbus

Genius 17355 points
Part Number: TPS549D22

Hello,

 

I have two questions for power sequence, specially about PMbus lines,  of TPS549D22.

 

1)

Due to the system requirement, power rail of PMbus pull-up is powered up before PVIN and VDD powering up.

Also it is powered down after PVIN and VDD powering down.

Is there any problem due to this power sequence? Could this power sequence damage the device?

2)

Can PMbus pull-up voltage be over PVIN and VDD voltage if pull-up voltage is under 5.5V?

Regards,

Oba