I have a question about UCC28251.
Please tell us the maximum duty cycle of OUTA and OUT B.
Best regards,
Takahiro Nishizawa
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Takahiro-san,
Duty cycle can be limited by the power stage (assuming the device is operating with closed loop feedback). Do you know how your customer is configuring the feedback to operate at different duty cycles? If they are hitting the cycle by cycle current limit, it will immediately terminate the current pulse. I would check the voltage at the ILIM pin to see if it is exceeding the 500mV threshold.
Best Regards,
Ben Lough
Hi Takahiro-san,
Yes, the max duty cycle of the high side and low side is 50% each. The LM5039 explains this in further detail in the Gate Driver Outputs section on page 16 of the datasheet:.
Best Regards,
Ben Lough