This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC256301: Variable power supply with UCC256301

Part Number: UCC256301

Can I make a variable DC-DC power supply with Output of  350V to 12V with UCC256301 by using a turns ratio of 1:1 for the transformer? The input is rectifier voltage from the mains.

  • Hello Tahir

    Please look at the calculator tool for this product on the device page at www.ti.com/.../technicaldocuments
    That will let you evaluate whether the LLC can operate over this wide range but to be honest the LLC wouldn't be able to operate over such a wide output voltage range (350:12 or 29:1). A better choice would be to use a full bridge or phase shifted full bridge - depending on your input voltage range.

    Regards
    Colin