This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54202H: Mistake in the datasheet of the part number TPS54202H

Part Number: TPS54202H


Hello,

I believe there is a mistake in the datasheet SLVSD26A–APRIL 2016–REVISED JANUARY 2017 of the part number TPS54202H.

In the figure: "Figure 16. 5-V, 2-A Reference Design" the values of the feedback resistors are wrong. If u make the design according to these values, u will get an output voltage of 7.31 V and not 5 V (feedback voltage is 0.596 V).

Best regards

Ondrej L.