This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ40Z50-R1: BMS total solution

Part Number: BQ40Z50-R1
Other Parts Discussed in Thread: BQ40Z50-R2

Hi there:

I'd like to purpose a total solution , include gauge, charging, cell balance to our customer, is there any reference design or prefer solution for following condition?

Cell type: LiFePo4 , 4 series with 3 parallel 

Charging current with 30A (10A each)

Charging voltage with 14.2V (min)

Discharge current: 200A min

cell balancing needed.

Or BQ40Z-50-R1 and BQ40Z50-R2 could reach that?