This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

WEBENCH® Tools/TPS62133: Schematic is different than in the datasheet.

Part Number: TPS62133
Other Parts Discussed in Thread: TPS62135

Tool/software: WEBENCH® Design Tools

When I compare the schematic of webench with the one from the datasheet I see that FSW (selection of switching frequency) is wired different.

Datasheet: to GND --> 2,5MHz

Webench: to output voltage --> first 2,5MHz until voltage is present or not working at all?

What is the purpous that FSW is connected to the output voltage? Or is this a bug? See both schematics below.