Hi,
II designed LiPo charging circuit using BQ24295. Circuit also can provide power to other circuits through USB.
I tried powering the circuit with a deeply discharged battery and load drawing 1A. I've 3 questions:
Question 1:
BQ is limiting input current to 1A always. If the load is drawing 1A, as expected, BQ is shutting down battery charging. So, it is evident that INLIM is set to 1A. I read back the register values, and this is what I got:
Input Source Control Register : 0b01011111
Power On Configuration Register : 0b00111011
Charge Current Control Register : 0b00100000
Pre Charge Termination Current Control Register : 0b00010001
Charge Voltage Control Register : 0b10110010
Charge Termination Control Register: 0b10011100
Boost Voltage Control Register: 0b10010011
Misc. Operation Control Register: 0b01001011
System Status Register: 0b10101100
Fault Register : 0b10000000
The resistor on ILIM pin is 150 Ohms. Can you please help me understand why BQ is behaving like this and what needs to be done to increase input current limit?
Voltage on ILIM pin is 0.3 VDC
Question 2:
I set the Fast charge current limit to 2A by writing 0x80 into REG02. It stays that way for a while (About 2 minutes) and will revert back to default value of 1A. What could be the reason for this behavior?
Question 3:
Boosted output is falling to 4.7V with no power from USB and load is drawing 1A. Is this because of the LiPo battery(1200mAh) itself?
I am attaching schematics for your reference.
Thanks
Teja