Hello,
I have a question about power sequence of UCD9090A, specially PMbus.
Due to thesystem requirement, PMbus pull-up power is powered up before V33D/V33A powering up.
(When powering down, V33D/V33A are shutdowned before PMbus pull-up power rail.)
So PMbus signals inputs go to 3.3V before V33D/V33A powering up.
Usually, digital device doesn’t accept higher voltage input than the device VDD.
Does this condition damage the device or cause any reliability issue?
Regards,
Oba