This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40428: Maximum current output support

Part Number: TPS40428


HI 

We are planning to use TPS40428 in our application :

VIN = 12V 
Vout = 0.8V to 0.9V with 0.85V (nominal)
Current = 50A Max
Programmable through I2C
Output voltage should be programmable
Enable option

Please confirm is it support 60A current and I2C bus interface?

Can we set default boot voltage without programming to 0.85V?