Hi I am using BQ25703A and want to set the default current to 4A when adapter is connected.
VILIM_HIZ (2.6V) = 1V + 40 * (VACP - VACN ) = 1+ 40 *IDPM *RAC
I could not find the value of IDPM.
if i Put the RAC as 7mOhms, will BQ25703A default input current limit change to 4A when adapter will be connected? On Power on my Microprocessor is off and i can not set register using i2c.