Other Parts Discussed in Thread: TPS22976
Hi
In our design I am using two independent and identical, charger (Bq25898) and battery (18650 - Li-Ion) configuration.
The system output (SYS) from each charger is tied together and connected to load.
MSP430 configures the charger devices independently. I use this configuration, to isolate the battery in case of failur.
I am planning to do isolation this by disabling the charger using CE# pin / EN_TERM (REG07.7) and by disabling BATFET.
In evm when I pulled up CE input the charger functionality is not halted, but the software configuration worked well. Please clarify?
I have following queries on the design too.
1. Is it recommended to tie the system outputs of two identical chargers together?
2. In case of failure in battery will it draw power from SYS through BATFET if is isolated by software by BATFET_DIS (REG09.5).
Thanks
Rejeesh S Raj