Hello,
Make board like as attached Webench circuit and test.
But output current is only 1.18A not 1.25A.
Test with changing input voltage from 50V to 52V. Output voltage is constant but Current is changed.
This circuit is not constant current circuit?
To get constant current, how can I change the circuit?
Regards,
Nicky
TPS92515HV_LED_2.975V_625mA_16S_2P.pdf
.