This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5165: Using LM5165X to generate negative -5V

Part Number: LM5165

I'm planning to use the LM5165X to generate a -5V supply rail.

Input is 24V+/-15% and output current min 10mA max 20mA.

Can I use a design as described in SLVA524 "Creating an Inverting Power Supply Using a Synchronous Step-Down Regulator"? with this regulator as well?

Kindly Mikael