Other Parts Discussed in Thread: BQSTUDIO, , GPCCHEM
Hello.
I use bq34z100-g1 (bqStudio 1.3.54.1 throw EV2300(v3.1r).) with 2S8P LiPol 3500mAh.
For my application best choise is Load Select =0 and Load Mode = 1.
The scheme contains:
- divider for BAT pin is 130k/16k
- measuring resistor = 10m
So I input in Data Memory next parameters:
Design Capacity | 28000 | MilliAmpHour |
Design Energy | 12600 | MilliWattHour |
Design Energy Scale | 8 | Number |
Qmax Cell 0 | 28000 | mAmpHr |
CC Gain | 10.123 | mohm |
CC Delta | 10.147 | mohm |
Voltage Divider | 9121 | mVolt |
After "Reset"-command "Registers" window shows me RC = 0 mAh, FCC = 164 mAh and SOC = 0% for Voltage = 8106 mV,
if I change Load Mode to 0 then RC = 21483, FCC = 25803, SOC = 84% for Voltage = 8106 mV.
Tell me, please, what I do wrong?
Vadim.