Other Parts Discussed in Thread: GPCCHEM
Hi,
I am currently using bq27421-G1A for my thesis design, I have encountered a problem during learning cycles.
The battery I am using is a 150mAh 4.2V LiCoO2-based rechargeable battery.
So I have no problem getting an Qmax update but during the last discharge cycle, where the resistance table is supposed to be updated, RES_UP and RUP_DIS are set at the same time. The battery is discharged at about -20mA, which is about C/7.5.
I am currently thinking about two possibilities:
- The battery chemistry does not match the gauge IC's pre-programmed profile;
- The discharge current is too small for a battery with small design capacity. I saw in another post that someone had the problem of getting RES_UP to set when they performed a learning cycle on a 300mAh battery, and they solved the problem by increasing discharge current to C/3. However, in my case, RES_UP can be set but just the RUP_DIS is set at the same time.
Could anyone shed some light on this and give me some guidance on how I can proceed?
Regards,
Kaylee