Other Parts Discussed in Thread: UCC28780,
Dear Sir,
I am looking at your solutions of ACF with UCC28780 and UCC24612.
I have a question about UCC24612-2
On page 12 of UCC24612 datasheet, there are such descriptions of
"For certain applications, this delay is essential for appropriate operation. In Active Clamp Flyback, especially when the primary side switches are using Si based super junction MOSFET, due to the large nonlinear junction capacitor, the SR often sees a leading spike current, follow by the real conduction current. Normally, a prolonged minimum on time can override this spike to make the circuit operate normally. However, this causes large negative current that transfer the energy from output to the input and reduces the overall converter efficiency"
I understand that the superjuction Fet has a very big variance of Coss in low Vds and high Vds. But i don't understand why it will cause leading edge spike so that you make UCC24612-2 to have prolonged turn on delay?
Are there any waveforms could help explain the leading edge spike?
Br