This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UC3846: Duty cycle of UC3846

Part Number: UC3846


I am testing UC3846 duty cycle at output with rotating potentiometer (by varying voltage) at EA pin EA(-). My maximum duty cycle is 38%. I am getting gradual change from 10% to 26% in duty cycle by rotating potentiometer at EA(-) pin. But after 26% it jumps to 38% directly. I changed the potentiometers & its values but the result is the same. Where is the mistake? Please help.

Thanks.

-Satyavijay