Hello
I have a question about PVIN specification of TPS549D22.
The datasheet defines that “recommended operating conditions” of PVIN is 1.5 – 16V.
For VDD, it is 4.5-20V. VDD has UVLO function, but PVIN doesn’t have UVLO.
During shutdown, the system requires TPS549D22 continue to output(around 1-1.2V) as long as possible.
In this case, VDD voltage can be kept over 4.5V relatively long time, but PVIN voltage can’t.
What will happen if VDD is over 4.5V but PVIN is under 1.5V?
My expectation is keeping output as far as possible.
Regards,
Oba