Other Parts Discussed in Thread: BQ27532-G1, BQ25895
Hi Team, i hope you can help me choosing the right ic's for circuit planning.
The application (Powerbank) needs the following features:
-Charging 1 Lithium Battery (3,7V/4,2V) with max. 2A (not removable/changeable) (at least 1A charging current)
-Power Path Management (support the system (load) with 5V power, while Battery is charging with less than 2A -> maybe remaining current from the 2A charging current)
-measuring state of charge with at least 10% accuracy, not sure if impedance track is necesarry for that, 4-6 LED displaying the State of charge
-only operate when load is added
-only QFP, QFN, DFN, SOP, SOIC or PLCC Packages
-optional integrated step up boost DC-DC converter for converting the Batteryvoltage to USB-Voltage 5V (Powerbank Output) at min. 1 - max. 2 A charging current
I already found the BQ27532-G1 with the BQ2425x for that application, but the BQ27532 is only available in DSBGA Package in Germany, witch is not an option.
Maybe you can recommend one or even multiple IC's for that application.
Is there a Solution where i dont need an additional microcontroller for driving the LED's?
Thanks for your help preaviously
with kind regards from Germany
Simon
-