Other Parts Discussed in Thread: BQ25896, , BQ25898C, BQ25898
Hi TI member
My customer use BQ25896 as master charger and BQ25898D as slave charger and BQ25898D D+/D- pins floating not connect.
For now the VBUS voltage changed by BQ25896 to 12V, but BQ25898D have no charge current and CHRG_STAT=00(Not charging)
I want to ask is that if the reg setting is default & VBUS=12V, can BQ25898D charge ? Or I need to modify the reg like 0x01 EN_12V & 0x02 disable AUTO_DPDM_EN reg?
Follow are customer read reg map:
[0x0]=0x48 [0x1]=0x1 [0x2]=0x9d [0x3]=0x1a [0x4]=0x20 [0x5]=0x13
[0x6]=0x5e [0x7]=0x8d [0x8]=0x3 [0x9]=0x44 [0xa]=0x74 [0xb]=0xa6
[0xc]=0x2 [0xd]=0x11 [0xe]=0x5d [0xf]=0x61 [0x10]=0x2d [0x11]=0xde
[0x11]=0xde [0x12]=0x0 [0x13]=0x8 [0x14]=0x15
Ibat=2048, Ilim=500, Vbus=12000, err=0, Ichg=0, Vbat=4164, ChrStat=0, CHGEN=1, VDPM=0
Thank you for read and help !
BR
Bruce