Hi,
my customer has a problem related to detection.
The circuit replicates the schematic of fig. 40 in datasheet with the change on Ctrm=220nF, because they need to make a longer soft start, due to low load, high current.
When they connect Vdd to the PSE, detection is never done at first tentative, but requires more than one.
Is this a normal situation?
Then they found a board that did make a detection only after an hour, so with a lot of tentatives..
Do you have any suggestion to verify and improve this situation.
Thanks
Umberto