Hello, I am working on a DC-DC converter with LM5116, it has 9-18V input and 7V output at maximum 8A.
Webench is connecting DEMB directly to GND, as I understand this is for starting the converter in a pre-biased load (diode emulation mode).
This is not the case in my application and the question is - should I keep it connected to GND or through a resistor to GND ? I see the eval board has both options. I have added a resistor in the design but I am not sure if it is better to install a zero ohm bridge or a resistor. And if a resistor is needed - how is the resistor calculated ?
And related to DEMB - the routing for this line should be made directly to the RSENSE GND via (and separated from the CSG trace) ? In the eval board it seems that the DEMB and CSG are tied together close to the LM5116 and then routed with a common route to RSENSE via.
The second issue is about the loop compensation network (between COMP and FB pins) - I have made some designs in Webench and for the same input I got significantly different values for the components in the compensation network. How can I check if the values are correct ? I tried to follow the explanation in the datasheet but it is not very clear to me.
Thank you,
Mihai