Other Parts Discussed in Thread: TPS706
Hi Guys,
I have a lot of fail on the TPS70933DRVR, there is no 3.3V out, it seem HI Z at the output.
The Vin is 3.66V and the current at 3.3Vout is 20mA
Cap at Vin is 1uF and Cap at Vout is 2uF.
The EN pin is floating
Let us know if you have an idea please or there a better part with same footprint for this application..?
Thanks again!
Regards