This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25703A: bq25703A / Resistor value on IADPT pin

Part Number: BQ25703A

Hi,

The customer plan to use 1uH inductor, and I understand that the recommended resistor value on IADPT pin is 93kohm for 1uH. Then please let me ask following two question.

  1. Can the resistor with 5% tolerance be used for this purpose?
  2. Can you recommend to use 100kohm for 1uH? 100kohm is reasonable value for customer.

Best Regards,

Satoshi / Japan Disty