This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCD9090A: PMBUS_CNTRL pin, pull-up

Genius 17525 points
Part Number: UCD9090A


Hello

 

I have a question for PMBUS_CNTRL pin for UCD9090A.

 

When configuring starting sequence by PMBUS_CNTRL and PMBUS_CNTRL pin is pulled-up, does the sequence is started correctly immediately after powering up?

 

My concern is that is “low-to-high rising edge” required to start sequence?

 

Regards,

Oba

 

  • PMBUS CONTROL is a level trigger instead of edge tripper.
    Remember that the polarity of the CONTROL is configured. it can start the sequencing either high or low of the PMBUS CONTROL.
    Regards
    Yihe