Part Number: LM2594HV
Dear support,
i was using LM2594HVM-3.3/NOPB in this configuration. It worked OK when supply was 24V, but it failed with burning smoke with supply on 48V.
I use it to power STM32F3 that runs on 3.3V.
Full schematic and gerbers attached.
Do you see some mistake why this would not work on 48V DC?
Since VIN leg was smoked blown away could it be that bigger cap is needed nea VIN leg?
What would be the problem. I attach schemeatic and photo of board.