How can I optimize the bq2060a for lead acid?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
You can set it up as a lithium chemistry. If it will be getting a float charge, then set up the self discharge as very low. Also, in that case, drop the Charge Efficiency a percent or two. You can set the Maintenance Charging Current to the desired limit for float charging, but note that there is no parameter specification for float charging voltage.