This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS25940: Can TPS25940 detect over current for reverse current flows from OUT terminal to IN terminal?

Part Number: TPS25940


 Hello guys,

 One of our customers is looking for a eFuse which can detect reverse overcurrent flowing from OUT terminal to IN terminal. Could you please tell me whether TPS25940 can detect the reverse overcurrent or not?

 Your reply would be much appreciated.

 Best regards,

 Kazuya Nakai.

 

  • Hi Kazuya Nakai,

    Can you please let us know the end equipment and the application use case?
    Yes, TPS25940 can detect reverse current from OUT to IN. The typical reverse current is reverse voltage /RON = 10mV/42mOhm = 238mA.
    When the reverse current exceeds 238mA (typ), the device turns OFF the internal FET.

    Best Regards
    Rakesh.
  • Hi Rakesh,

    Thank you very much for your prompt reply. I could understand the reverse current blocking function well because of your reply.
    I'm afraid I can't tell you this application because the customer haven't disclosed it to us yet.

    Thank you very much again and best regards,
    Kazuya Nakai.